Other Parts Discussed in Thread: CC2640
Hi,
I'm using the SimpleBLEObserver Project.
I tried to write and read some values to SNV memory but failed with return value of FAILURE / INVALID PARAMETER.
But in SimpleBLECentral project, it is working which means writing and reading to SNV memory is OK.
Is there any limitation on SNV api with SimpleBLEObserver project?
Environment
TI-RTOS version : 2.13.00.06
BLE SDK version no. : 2.01.00.44423
MCU : CC2640
Test codes
void snv_test(void)
{
uint8_t snv_test_wb[5]={1,}, snv_test_rb[5]={0,};
uint8_t get_result;
static uint8_t sample_data=1;
snv_test_wb[0] = sample_data;
get_result = osal_snv_write(0x81, sizeof(snv_test_wb), snv_test_wb);
get_result = osal_snv_read(0x81, sizeof(snv_test_rb), snv_test_rb);
sample_data++;
}