Other Parts Discussed in Thread: CC2541
Hi
I am a beginner in BLE.
I want to configure HM-10 (having cc2541) as a master. For this I am referring to SimpleBLECentral.
I want to have an additional functionality that if the master is connected to the slave an Led on P1_0 should glow.
If the master gets disconnected with the slave or if the master is not connected to the slave , the led on P1_0 should not glow.
Kindly provide me the exact lines of code reg this functionality and let me know where to place it in the existing code . Also, Let me know if any additional header files have to be included.
Let me know if there is any app on playstore (for android) to check the connection between master and slave configurations ( BLE HM-10 having cc2541).
Thanks
Ankur