I am having two HM-10 (each having cc2541) . I have configured one hm-10 as a slave by downloading simpleBLEPeripheral example on one HM-10 after disabling the power saving. I could pair it with my mobile phone using 000000 as the pin key.
I have downloaded simpleBLECentral on another HM-10 so that I can use it as a master . Please let me know if I have to make any change in simpleBLECentral so that it can pair with the slave. The simpleBLECentral has a default pass code as 19655. I guess I need to change this to 00000. Kindly correct me if I am wrong.
Also let me know can I check whether the master and slave are connected. Is there any app on the playstore for android phones.