4403.HOGP Log 10-04-16 (1).psdThis thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
4403.HOGP Log 10-04-16 (1).psdYuri,
The log attached does not have all the samples up to P.nbr. = 7401 that you have highlighted in the screenshot above. Can you please verify that the screenshot is from the same log file?
Best regards,
Vihang
Hello!
Thank you for your responses,
Zahid,
The enviroment of the tests is not noisy at all, in fact the only transmission is done by the BT, therefore,
i think this is not the reason.
Vihang,
I will create new sniffer and log files to make sure that they match and post them here.
Thank you,
Hi,
No problem, I will do as you say.
I will have the new logs for you by the end of tomorrow.
Hello Vihang!
Unfortunately, I haven't had a chance to log the events yet,
I will post the new log as soon as possible,
Yuri.
Hello Vihang!
Here is the new log that includes the information you have requested.
This is mouse movement from left to right every 55 milliseconds. i have stopped the logger as soon as i saw serious deviation from the original points
where the mouse appeared. New Log for TI Forum.rar