Other Parts Discussed in Thread: CC2650, BLE-STACK
Hi,
i'm using a CC2650 connected via SPI with a EFM32 and the SNP example. At the moment i've a problem with changing the advertising device name.
I try to change the complete local name to "Test" by set the advertisement data over the npi command. I'm using 0x09 as advertising data-type and change it for the scan response data and also for the non-connectable advertisement data. But instead of changing the complete local name it changes the shortened local name. The device name remains SNP. I also tried 0x08 as advertising data-type.
Have i to do other things to change the device name of the SNP-Application?