Hi,
I'm experience a strange and annoying issue with CC2541.
My Images are asymmetric and Image A is larger than Image B.
Updating Image B from Image A works but updating Image A from B doesn't; the Image is correct ( jtag read back) but the CRC verification fails.
The CRC verification fails also if I append Image A ((jtag) when Image B is already flashed but it passes when only bootloader and Image A are present.
It's quite strange and also a big problem for us, can anyone help debugging it?
Thanks
Paolo
Here's my xcl configuration for Image A
////////////////////////////////////////////////////////////////////////////////
//
// Segment limits
//
//
// XDATA available to the program.
//
-D_XDATA_BEG=0x0000
-D_XDATA_END=0x1EFF
//
// The 8052 IDATA is overlayed on the SoC XDATA space from 0x1F00-0x1FFF.
//
-D_IDATA_BEG=0x0A // Must reserve 0x08-0x09 for the IBM INTVEC re-direct.
-D_IDATA_END=0xFF
//
// CODE
//
-D_CODE_BEG=0x0830 // First page is for the IBM which intercepts the H/W INTVECS.
-D_CODE_END=0x4FFF // Next 7 pages of Bank 0.
//
-D_BANK4_BEG=0x48800 // Last 10 pages of Bank 4.
-D_BANK4_END=0x4FFFF
//
-D_BANK5_BEG=0x58000
-D_BANK5_END=0x5FFFF
//
-D_BANK6_BEG=0x68000
-D_BANK6_END=0x6FFFF
//
-D_BANK7_BEG=0x78000
// Cannot use the lock-bits page in a boot-loadable image; skip NV pages area.
-D_BANK7_END=0x7E7FF
//
// Register bank setup
//
-D?REGISTER_BANK=0 // Default register bank (0,1,2,3).
-D_REGISTER_BANK_BEG=0 // Start address for default register bank (00,08,10,18).
//
// PDATA page setup
//
-D?PBANK_NUMBER=00 // High byte of 16-bit address to the PDATA area.
//
// Virtual register setup
//
-D_BREG_BEG=0x00 // The bit address where the BREG segments starts.
// Must be placed on: _BREG_BEG%8=0 where _BREG_BEG <= 0x78.
-D?VB=0x20 // ?VB is used when referencing BREG as whole byte.
// Must be placed on: ?VB=0x20+_BREG_BEG/8.
////////////////////////////////////////////////////////////////////////////////
//
// IDATA memory
//
// Setup "bit" segments (only for '__no_init bool' variables).
-Z(BIT)BREG=_BREG_BEG
-Z(BIT)BIT_N=0-7F
-Z(DATA)REGISTERS+8=_REGISTER_BANK_BEG
-Z(DATA)BDATA_Z,BDATA_N,BDATA_I=20-2F
-Z(DATA)VREG+_NR_OF_VIRTUAL_REGISTERS=_IDATA_BEG-7F
-Z(DATA)PSP,XSP=_IDATA_BEG-7F
-Z(DATA)DOVERLAY=_IDATA_BEG-7F
-Z(DATA)DATA_I,DATA_Z,DATA_N=_IDATA_BEG-7F
-U(IDATA)0-7F=(DATA)0-7F
-Z(IDATA)IDATA_I,IDATA_Z,IDATA_N=_IDATA_BEG-_IDATA_END
-Z(IDATA)ISTACK+_IDATA_STACK_SIZE#_IDATA_BEG-_IDATA_END
-Z(IDATA)IOVERLAY=_IDATA_BEG-FF
////////////////////////////////////////////////////////////////////////////////
//
// ROM memory
//
-Z(CODE)CHECKSUM=0x0800-0x0801
-Z(CODE)IMAGE_HEADER=0x802-0x80F
-Z(CODE)AES_HEADER=0x810-0x82F
-Z(CODE)INTVEC=_CODE_BEG-_CODE_END
-Z(CODE)BIT_ID,BDATA_ID,DATA_ID,IDATA_ID,IXDATA_ID,PDATA_ID,XDATA_ID=_CODE_BEG-_CODE_END
-Z(CODE)CSTART,RCODE,DIFUNCT,NEAR_CODE=_CODE_BEG-_CODE_END
-Z(CODE)BANK_RELAYS=_CODE_BEG-_CODE_END
-D_SLEEP_CODE_SPACE_START=(_CODE_END-7)
-D_SLEEP_CODE_SPACE_END=(_CODE_END)
-Z(CODE)SLEEP_CODE=_SLEEP_CODE_SPACE_START-_SLEEP_CODE_SPACE_END
//
// Setup for constants located in code memory:
//
-Z(CODE)CODE_C=_CODE_BEG-_CODE_END
//
// Define segments for const data in flash.
// First the segment with addresses as used by the program (flash mapped as upper XDATA)
-P(CONST)XDATA_ROM_C=0x8000-0xFFFF
//
// Then the segment with addresses as put in the hex file (flash bank 5).
-P(CODE)XDATA_ROM_C_FLASH=_BANK5_BEG-_BANK5_END
//
// Finally link these segments (XDATA_ROM_C_FLASH is the initializer segment for XDATA_ROM_C,
// we map the flash in the XDATA address range instead of copying the data to RAM)
-QXDATA_ROM_C=XDATA_ROM_C_FLASH
-Z(CODE)ALIGNED_CODE|2=_CODE_BEG-_CODE_END,_BANK4_BEG-_BANK4_END,_BANK5_BEG-_BANK5_END,\
_BANK6_BEG-_BANK6_END,_BANK7_BEG-_BANK7_END
-P(CODE)BANKED_CODE=_CODE_BEG-_CODE_END,_BANK4_BEG-_BANK4_END,_BANK5_BEG-_BANK5_END,\
_BANK6_BEG-_BANK6_END,_BANK7_BEG-_BANK7_END
////////////////////////////////////////////////////////////////////////////////
//
// XDATA memory
//
-Z(XDATA)XSTACK+_XDATA_STACK_SIZE=_XDATA_BEG-_XDATA_END
-Z(XDATA)XDATA_Z,XDATA_I,PDATA_Z=_XDATA_BEG-_XDATA_END
-P(XDATA)XDATA_N=_XDATA_BEG-_XDATA_END
-cx51
////////////////////////////////////////////////////////////////////////////////
//
// Misc.
//
//
// Offset fix for the unconventional bank numbering for this SOC (root bank is callled "bank 0").
-D_FIRST_BANK_ADDR=0x10000
//
// NOTE: The -M option below is needed when linker output should be in "intel-extended" (HEX)
// file format for banked code model. It translates the logical addresses for the EW8051
// to physical addresses in the output file format. Without this, the HEX output file will
// include 32 kB blocks of zero bytes/gap in between each code bank.
//
-M(CODE)[(_CODEBANK_START+_FIRST_BANK_ADDR)-(_CODEBANK_END+_FIRST_BANK_ADDR)]*_NR_OF_BANKS+0x10000=\
0x8000
// When -M is used to build debug output, XLINK gives warning [w69] which is safely ignored.
-ww69=i
// When INTVEC is relocated, XLINK gives error [e18] which is safely ignored.
-we18=i
//
// Fill code gaps with 0xFFFF for monolithic binary file with no addressing.
//
-HFFFF
//
// Skip CRC & SHDW when calculating the CRC.
//
-J2,crc=8005,=0804-_BANK7_END
//
////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
Here's my xcl configuration for Image B
////////////////////////////////////////////////////////////////////////////////
//
// Segment limits
//
//
// XDATA available to the program.
//
-D_XDATA_BEG=0x0000
-D_XDATA_END=0x1EFF
//
// The 8052 IDATA is overlayed on the SoC XDATA space from 0x1F00-0x1FFF.
//
-D_IDATA_BEG=0x0A // Must reserve 0x08-0x09 for the IBM INTVEC re-direct.
-D_IDATA_END=0xFF
//
// CODE
//
-D_CODE_BEG=0x5030 // Last 7 pages of Bank 0.
-D_CODE_END=0x7FFF
//
-D_BANK1_BEG=0x18000
-D_BANK1_END=0x1FFFF
//
-D_BANK2_BEG=0x28000
-D_BANK2_END=0x2FFFF
//
-D_BANK3_BEG=0x38000
-D_BANK3_END=0x3FFFF
//
-D_BANK4_BEG=0x48000
-D_BANK4_END=0x487FF // First 6 pages of Bank 4.
//
// Register bank setup
//
-D?REGISTER_BANK=0 // Default register bank (0,1,2,3).
-D_REGISTER_BANK_BEG=0 // Start address for default register bank (00,08,10,18).
//
// PDATA page setup
//
-D?PBANK_NUMBER=00 // High byte of 16-bit address to the PDATA area.
//
// Virtual register setup
//
-D_BREG_BEG=0x00 // The bit address where the BREG segments starts.
// Must be placed on: _BREG_BEG%8=0 where _BREG_BEG <= 0x78.
-D?VB=0x20 // ?VB is used when referencing BREG as whole byte.
// Must be placed on: ?VB=0x20+_BREG_BEG/8.
////////////////////////////////////////////////////////////////////////////////
//
// IDATA memory
//
// Setup "bit" segments (only for '__no_init bool' variables).
-Z(BIT)BREG=_BREG_BEG
-Z(BIT)BIT_N=0-7F
-Z(DATA)REGISTERS+8=_REGISTER_BANK_BEG
-Z(DATA)BDATA_Z,BDATA_N,BDATA_I=20-2F
-Z(DATA)VREG+_NR_OF_VIRTUAL_REGISTERS=_IDATA_BEG-7F
-Z(DATA)PSP,XSP=_IDATA_BEG-7F
-Z(DATA)DOVERLAY=_IDATA_BEG-7F
-Z(DATA)DATA_I,DATA_Z,DATA_N=_IDATA_BEG-7F
-U(IDATA)0-7F=(DATA)0-7F
-Z(IDATA)IDATA_I,IDATA_Z,IDATA_N=_IDATA_BEG-_IDATA_END
-Z(IDATA)ISTACK+_IDATA_STACK_SIZE#_IDATA_BEG-_IDATA_END
-Z(IDATA)IOVERLAY=_IDATA_BEG-FF
////////////////////////////////////////////////////////////////////////////////
//
// ROM memory
//
-Z(CODE)CHECKSUM=0x5000-0x5001
-Z(CODE)IMAGE_HEADER=0x5002-0x500F
-Z(CODE)AES_HEADER=0x5010-0x502F
-Z(CODE)INTVEC=_CODE_BEG-_CODE_END
-Z(CODE)BIT_ID,BDATA_ID,DATA_ID,IDATA_ID,IXDATA_ID,PDATA_ID,XDATA_ID=_CODE_BEG-_CODE_END
-Z(CODE)CSTART,RCODE,DIFUNCT,NEAR_CODE=_CODE_BEG-_CODE_END
-Z(CODE)BANK_RELAYS=_CODE_BEG-_CODE_END
-D_SLEEP_CODE_SPACE_START=(_CODE_END-7)
-D_SLEEP_CODE_SPACE_END=(_CODE_END)
-Z(CODE)SLEEP_CODE=_SLEEP_CODE_SPACE_START-_SLEEP_CODE_SPACE_END
//
// Setup for constants located in code memory:
//
-Z(CODE)CODE_C=_CODE_BEG-_CODE_END
//
// Define segments for const data in flash.
// First the segment with addresses as used by the program (flash mapped as upper XDATA)
-P(CONST)XDATA_ROM_C=0x8000-0xFFFF
//
// Then the segment with addresses as put in the hex file (flash bank 4).
-P(CODE)XDATA_ROM_C_FLASH=_BANK4_BEG-_BANK4_END
//
// Finally link these segments (XDATA_ROM_C_FLASH is the initializer segment for XDATA_ROM_C,
// we map the flash in the XDATA address range instead of copying the data to RAM)
-QXDATA_ROM_C=XDATA_ROM_C_FLASH
-Z(CODE)ALIGNED_CODE|2=_CODE_BEG-_CODE_END,_BANK1_BEG-_BANK1_END,_BANK2_BEG-_BANK2_END,\
_BANK3_BEG-_BANK3_END,_BANK4_BEG-_BANK4_END
-P(CODE)BANKED_CODE=_CODE_BEG-_CODE_END,_BANK1_BEG-_BANK1_END,_BANK2_BEG-_BANK2_END,\
_BANK3_BEG-_BANK3_END,_BANK4_BEG-_BANK4_END
////////////////////////////////////////////////////////////////////////////////
//
// XDATA memory
//
-Z(XDATA)XSTACK+_XDATA_STACK_SIZE=_XDATA_BEG-_XDATA_END
-Z(XDATA)XDATA_Z,XDATA_I,PDATA_Z=_XDATA_BEG-_XDATA_END
-P(XDATA)XDATA_N=_XDATA_BEG-_XDATA_END
-cx51
////////////////////////////////////////////////////////////////////////////////
//
// Misc.
//
//
// Offset fix for the unconventional bank numbering for this SOC (root bank is callled "bank 0").
-D_FIRST_BANK_ADDR=0x10000
//
// NOTE: The -M option below is needed when linker output should be in "intel-extended" (HEX)
// file format for banked code model. It translates the logical addresses for the EW8051
// to physical addresses in the output file format. Without this, the HEX output file will
// include 32 kB blocks of zero bytes/gap in between each code bank.
//
-M(CODE)[(_CODEBANK_START+_FIRST_BANK_ADDR)-(_CODEBANK_END+_FIRST_BANK_ADDR)]*_NR_OF_BANKS+0x10000=\
0x8000
// When -M is used to build debug output, XLINK gives warning [w69] which is safely ignored.
-ww69=i
// When INTVEC is relocated, XLINK gives error [e18] which is safely ignored.
-we18=i
//
// Fill code gaps with 0xFFFF for monolithic binary file with no addressing.
//
-HFFFF
//
// Skip CRC & SHDW when calculating the CRC.
// -J2,crc=8005,= D_CODE_BEG of cc254x_f256_imgB.xc + 4 -_BANK4_END
-J2,crc=8005,=5004-_BANK4_END
//
////////////////////////////////////////////////////////////////////////////////
BIM Main.c defines:
#define BIM_IMG_A_PAGE 1
#define BIM_IMG_A_AREA 69
#define BIM_IMG_B_PAGE 10
#define BIM_IMG_B_AREA (124 - BIM_IMG_A_AREA)
#define BIM_CRC_OSET 0x00
#define BIM_HDR_OSET 0x00