File inc/hw_memmap.h from ti-cc26xxware driverlib pack contains set of NONBUF_BASE definitions:
#define SSI0_NONBUF_BASE 0x60000000 // SSI CPU nonbuf base #define UART0_NONBUF_BASE 0x60001000 // UART CPU nonbuf base #define I2C0_NONBUF_BASE 0x60002000 // I2C CPU nonbuf base
...
Driverlib code uses these definitions in some places. But I wasn't able to found what these registers are and what the difference with the usual peripherals (started from the 0x40000000 address).
So, my question is: what is the NONBUF_BASE definitions and when I have to use them?
BR, Andrey.