Other Parts Discussed in Thread: CC2564
I just wanted to clarify what is meant by the parameter 'Maximum Usable Input Power' in section 5.7.4.1.1 Bluetooth Receiver—In-Band Signals of CC2564's datasheet. It is stated there that the -5 dbm is the maximum usable input power. Does this mean that I cannot input a power greater than -5dbm in the RF pin of the module? What would be the effect to the receiver in case the input signal power is beyond that limit?