This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't resolve linkDB_Find()

Other Parts Discussed in Thread: CC2640

We are attempting to determine if the connected Central is in our Peripheral's bond list using a CC2640.  When the ble connection is established, we call linkDB_Find() with the connection handle.  unfortunately, CCS Version 6.1.3, compiler version TI v5.2.4 [TI v5.2.7] fails during linking with undefined symbol for linkDB_Find.  We can find the header for the function in linkdb.h" and have added the include file.  However, the error persists.  We see this function used in gapbondmgr.c as well.  Any help would be greatly appreciated.

#include "linkdb.h"

linkDBItem_t *link = linkDB_Find( gapConnHandle ); //find link database entry

if (link)
 uint8 idx = GAPBondMgr_ResolveAddr( link->addrType, link->addr, resolv_addr ); //find bond mgr index

  • Hello,

    You don't need to call linkDB_Find in order to call GAPBondMgr_ResolveAddr. The addr type and device address can be obtained from GAPRole params: GAPROLE_BD_ADDR_TYPE and GAPROLE_BD_ADDR.

    Best wishes