Hi,
i am using the CC2640 based on the simpleBLEPeripheral project example and i am trying to OAD with BLE Device Monitor and CC2540 USB Dongle.
On the BLE Device Monitor i can connect to the CC2640.
If i try to use the OAD and selet the .hex file press start i get this:
After this the CC2640 crashes too.
Any idea?
First i flash the simpleBLEPeripheralStack then the App and then the bim_extflash to the CC2640.
If i use the sensortag app on the iphone, the OAD gets stuck on 0% and doenst do any downlaod at all.