This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

simple_peripheral BLE stack2.2



Hi,

I am trying to venture into BLE stack 2.2. I am using CCS6.1.2 I am working with the CC2650DK at this time. I was able to compile and download the stack project to the DK. I am able to compile the simple_peripheral project but I get a debug error. I notice the simple_peripheral project doesn't have a targetConfigs directory. I have attached a screenshot below for pointers. I did install the TIRTOS 2.18 separately and then installed the BLE stack 2.2 later. If this is an installation problem, where will I find the installation logs? 

Thanks,

Priya