Hi,
I have some homebrew code (an OS that makes register level calls) that was taken and modified based on the CC2541 ble stack that I would like to run on the CC2650 processor and make calls to the CC2650 ble stack. I understand that this will be very difficult. Where can I go to specifically find the software differences between the two stacks and why this would be difficult, in case I wanted to pursue this or needed to explain it to someone else? (is there documentation specifically for the differences?) The feedback I have so far is: this will be very very difficult, less about how it would be difficult.
Thanks for all the help!
Code2e