This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

In CC2650 can i use ZIgbee and Bluetooth same time?

Other Parts Discussed in Thread: CC2650

Hi,

I'm planning to use  CC2650 module in my IOT application, please can anyone give the answer to the below quires: 

1). Can anyone tell me i can use both zigbee & bluetooth same time?

2). What is the maximum distance both zigbee and bluetooth will support?

3). I can see only two line given for power amplifier interface, is it for zigbee/bluetooth

Looking forward reply.

Thanks,

Chandu

 

  • H Chandu,

    1) Currently you cannot run Zigbee and connected BLE concurrently. A combination of Zigbee and BLE broadcasting is possible.

    2) Maximum range will depend on the antenna, board size, environment, etc. Typically you can easily get multi-room indoor coverage and 100 m outdoor line of sight.

    3) I am not sure which signals you are reffering to here.

    Cheers,

    Fredrik