This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLE Device Monitoring v2.20 is not working with CC2650LP

Other Parts Discussed in Thread: CC2540, CC2640, CC2650

Hello Team,

I am working for a customer with BLE example spp_ble_server. Customer has two CC2650LP so They have programmed application in One LaunchPAD and other one They wish to use with BLE device monitor / B-Tool. For using this with BLE device monitor, I have programmed below code in CC2650LP from ../Texas Instruments\SmartRF Tools\BLE Device Monitor\firmware\cc26xx\launchpad folder:

1. CC2650LaunchPad_BLE_All_v1_00.hex

2. CC2650LaunchPad_BLE_App_v1_00.hex

Now I have connected it with BLE device monitor and assign launchPAD application COM port with 115200 Baud rate +  Flow control NONE. I am getting error No response from BLE Host at COM6.  I could use CC2540 USB with Host test program on the same BLE device monitor but problem with this configuration that I can't send more than 18-19 bytes while I wish to send 40 bytes. As per me with CC2640 (BLE 4.2 support) it is possible. Please advise if I am right here.. and help me in connecting CC2650LP with BLE device monitor.

Regards,

Vikas Chola