This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-RTOS example doesn't work with CCS 6.2

Other Parts Discussed in Thread: CC2650STK

I use the CC2650STK and the SensorTag Debugger DevPack (XDS110). I would like to start my first project with the SimpleLink Academy TI-RTOS example.

I can built and debug the programm. After the debug-process the programm seems to run but the LED isn`t blinking. If i want to press the suspend button (Alt+F8), then i get the following error:

Cortex_M3_0: Trouble Halting Target CPU: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK) (Emulation package 6.0.407.3)