Other Parts Discussed in Thread: CC2650
Hi,
I am using CC2650 to send out advertising packet every 100ms.
When I use ubertooth to capture the data packet, I found that some adv packets are not transmitted out.
Here is the capturing result.
Adv type is 6, interval is 113.250ms
Adv type is 6, interval is 330.895ms
Adv type is 6, interval is 113.120ms
Adv type is 6, interval is 109.061ms
Adv type is 6, interval is 104.866ms
Adv type is 6, interval is 111.001ms
Adv type is 6, interval is 104.803ms
Adv type is 6, interval is 111.149ms
Adv type is 6, interval is 106.961ms
Adv type is 6, interval is 104.864ms
Adv type is 6, interval is 115.354ms
Adv type is 6, interval is 219.175ms
We can see one or two adv packets are not transmitted out almost in every 10 packets.
Is there anything would cause the adv packet not sent out?