Hi Everyone!!!
I am developing a custom board based on CC2650. I am referring to the designs given by TI:
A) SensorTag(document: tidu862)
B)CC2650 Development Kit
Following are my doubts:
1) In tidu862, pins 1(RF_P) & 2(RF_N) are connected to antenna circuit via 15pF caps & there is no cap connected to inductor L2 whereas in CC2650EM-7ID schematic (available on ti's site), those pins are connected directly to antenna circuit & L11 inductor is connected in series to a capacitor C31 of value 6.8pF.
(a) Which to follow?
(b) What are the advantages/disadvantages in either?
2) It is mentioned in Technical Ref. Manual(TRM) of CC2650(document: swcu117f) on pg 26 & 413 that to have lowest power, connect VDDR to internal DC-DC, which is pin DCDC_SW. In this case:
(a) VDDS_DCDC should be connected to VDDS?
(b) VDDR & VDDR_RF should be shorted?
(c) VDDR/VDDR_RF should be connected directly to DCDC_SW?
(c) The decoupling capacitor(s) connected to VDDR & VDDR_RF shown in either of the above mentioned documents should be still connected?
3) Also, it is mentioned in TRM that if Global_LDO is used to supply to VDDR, VDDR & VVDR_RF should be shorted & DCDC_SW should be left floating. Then:
(a) Why in reference designs, DCDC_SW is connected to VDDR, VDDR_RF through an inductor of 10uH?
(b) What exact differences(pin connections) are there in either mode: Internal DCDC & Global LDO ?
Please Help Me!
- Prasad.