Hi
I just got the CC2650 development board and it works with the TI app (only shows device info), so now I am trying to have it working with some app.
I need to build an app which can send some simple commands to the cc2650 and gets a reply.
For start I tried using existing bluetooth apps from the android app store, like the bluetooth terminal app.
None except the TI app are able to connect to the CC2650, all of them fail when trying to connect.
What do I need to do so that I am able to send characters from one of the bluetooth serial console apps to the CC2650 and have it reply something?
Or is there a better way of testing such functionality without developing a stand alone app from scratch (using the TI app as template)?
Or does the TI app have some functionality where I can try manually sending data packets?