This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLE Stack 2.0.2 is it possible that it doesn't run on older CC2640 running fine on 1.4 ?

Other Parts Discussed in Thread: CC2640, CC2541, CC2540, BLE-STACK, CC2650

Hi there,

we do see VERY weird bahavior of the new Stack e.g. the wrong BLE address is send over radio and a single change of the Device Name stops the software to work.

We NEED to know what is going on

Thanks

  • Hi Ralph,

    Are you running the BLE SDK 2.2 on a TI dev kit or custom hardware?

    Are you using an example project from the BLE SDK? I would recommend starting with one of the BLE SDK v2.2 example projects (like SimpleBLEPeripheral) and adding any modifications after verifying that the default projects work.

    Another option would be going through SimpleLink Academy and running ProjectZero.
  • Hi Rachel,

    I am using CC2640 since 2014 under NDA and have some designs already in mass production.
    All the simpler things I have done with stack 2.0 and 2.1 don't work with 2.2
    I have weird results as well as some other here in E2E.
    I have to get running this project until this weekend, and I tell you that the stack 2.2 is not useable at all.

    This will be my last project using TI. I will switch over to Nordic for sure. My request about these bunch of problems I have are unanswered since 6 weeks as well as the one from other engineers.

    I did learn programming using Texas Instrumenst TI 9900 cpu's back in 1982 and have always been a TI fan. But what I see now with stack 2.2 is the proof that TI lost connection.

    However, I can not believe that it ends like this. I have setup TWO computers the past weekend one WIN 10 other WIN 7 to check out if it is related to operating system. But on both computers the same.

    With stack 2.2 debugging is not possible, as soon as you use the pragma to switch off optimization for one single function, the whole code does not run at all. I am used to that general optimization off does not work, but in 2.1 I could at least use the pragma to control optimization for parts of the code.

    If you use advertising strings longer then 21byte, nothing works
    if you change the length of the scan response string it works sometimes, sometimes not ( depends if you change lenght even or uneven bytes).

    The new issue I am despair on is the following:

    I delivered two of my board to my customer, these boards ran fine here with stack 2.1 code and held one board back for remote developing.

    My hardware design I am using is the same running fine in a mass production product.

    I am using the SPB sample project (stack 2.2) as base. The original SBP runs with no issues on all three boards.

    If I add some files and make the simple_peripheral.c, and references, local in workspace, the same code runs fine on one board but does not run on the others.

    not only this, if I run a code verification after the boards were powered for >20min the boards which don't run fail in code verification.
    So either the chip flash 'forgets' programming or the stack 2.2 makes changes to the flash. Reprogramming the chip passes verification, but code does not run.
    Reprogramming the unchanged SBP project runs fine for hours and days. But any code changed just a little bit does not and flash content alters after a while.
    And not only this, on one of the boards I got the code running once, BUT the chip send a wrong BLE address over air. It was not the same you read out with FP2, the last byte was supposed to be an B2 but sent was A2. Reading with FP the address remains ending with B2.

    So Stack 2.2 seems really sick to me. I am not a newcomer with the CC2640 and I do want to know the reason.
    I have been posting a view issues in the past 6 weeks like others and none of the experienced TI'ers responded. This is to me a sign that there is something serious wrong.

    So either find somebody who has the balls to say 'stay away from 2.2 for the moment' or tell us what is wrong.

    From my view and situation, there is one last issue as a possible explanation. The CC2640 I am using I did buy in 2015. they are PG2 for sure but not sure about .1

    So question remains, is it possible that these chips are too old for stack 2.2 ?

    Ah ja I forgot, going back to stack 2.1 works fine on all boards ....

    Good luck

  • It's confusing in your description. As I remember, there is no BLE stack version 2.0.2 or 1.4 for CC26xx. You can check www.ti.com/.../BLE-STACK-ARCHIVE first. I suppose the stack version 1.4 is BLE-STACK V1.4.0 (Support for CC2540/CC2541) and it is not for CC26xx.
  • sorry I mixed that up with the 2540, I have edited my post, it is 3am here and I am exhausted finding a solution for my customer
  • If you use CC2540. the latest BLE Stack for it is version 1.4.2 which you can download it from www.ti.com/.../ble-stack . Please note version 2.2 is for CC26XX.
  • I USE CC2640 and latest stack 2.2 IS USELESS !!!

    can somebody go into the details please ?
  • Can you specify how you advertising strings longer then 21byte?
  • By the way, the scan response data can't be larger than 31 bytes and GAP_NAME_LENGTH in gattgattserver.h that gives a max length of 21 bytes which is part of the BLE spec. You can refer to the discussions in e2e.ti.com/.../355230
  • Just to end this discussion.

    The weird things I am experiencing are related to my own custom board. However I am reusing a layout design which is in production in another earlier project I developed. So I trusted my design too much.

    Stack 2.2 IS NOT USELESS

    However one thing, which is the root for the loss of confidence in the new stack is discussed here:

    What I now experienced with my CC2640 4x4 design is that these chip seem to die over time and programming cycle. I have seen that after any reprogramming the issues got worth and worth.

    What is sad and funny at the same time is that the very first programmed out of the box SBP still can be programmed and runs fine. Any other code does not run and the board I used the most finally can even not be programmed any more. I could see this effect over more then 10 boards now.

    I bought these chips over a year ago, and now I assume, that they might have been affected by moisture and a rough handling in prototype soldering process or important related parts like the crystals might be affected.

    What I have experienced until the board died was very similar like in this discussion

    Finally I tried my code on the Launchpad board, and it works there. I have changed the board and chip type to CC2640 4x4 and on the Launchbad sit´s a CC2650. So it might be interesting if anybody has used the 4x4 chip and just changing the chip type in ble_user_config.c to the custom board did work for him.

     I will assemble new boards with fresh chips in the coming days and see if I can get this to work and report my results here.

    Sorry for being harsh about TI and the new stack, but looking at the prices for 1000pcs lots does create a certain negative moot as well .....

    Good luck for your work

    Ralph