This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI CC2640 wireless communication with Windows application

Other Parts Discussed in Thread: CC2640, CC2650, CC2541EMK, CC2540

Hello,

I'm making a device with CC2640 and 2 sensors onboard a custom PCB. I want to fetch the data sent over BLE on a windows or maybe a linux system, Can I do that using the inbuilt bluetooth of laptop? Since it's a BLE device so am not sure whether it's possible.

I'm hoping it's possible without any extra dongle after reading this article:  msdn.microsoft.com/.../jj159880(v=vs.85).aspx

Can anyone tell if it's possible or would I need to use any extra dongle like ones from bluegiga?

If not then is the same possible using cc2650 using IEEE 802.15.4 ?

Thanks in Advance.

-

Anurag