Hi Ti team,
I have some questions with scanning interval and window during scanning state and initiating state.
On Core v4.2 spec, the following scanning related things are mentioned. And the scanning stops before initiating a connection by using general, directed, auto, or selective connection establishment procedure.
1. Tgap(gen_disc_scan_min), 10.24s, minimum time to perform scanning when performing the general discovery procedure.
2. Tgap(lim_disc_scan_min), 10.24s, minimum time to perform scanning when performing the limited discovery procedure.
3. Tgap(lim_disc_scan_int), 11.25ms, scan interval used in the limited discovery procedure
4. Tgap(scan_fast_period), 30.72s, minimum time to perform scanning when user initiated.
5. Tgap(scan_fast_interval), 30ms to 60ms, Scan interval in any discovery or connection establishment procedure when user initiated.
6. Tgap(scan_fast_window), 30ms, Scan window in any discovery or connection establishment procedure when user initiated.
7. Tgap(scan_slow_interval1), 1.28s, Scan interval in any discovery or connection establishment procedure when background scanning
8. Tgap(scan_slow_window1), 11.25ms, Scan window in any discovery or connection establishment procedure when background scanning
9. Tgap(scan_slow_interval2), 2.56s, Scan interval in any discovery or connection establishment procedure when background scanning
10. Tgap(scan_slow_window2), 11.5ms, Scan window in any discovery or connection establishment procedure when background scanning
But, on swru393d,
11. TGAP_GEN_DISC_SCAN, 10240ms, Time (ms) to perform scanning for general "discovery" procedure.
12. TGAP_LIM_DISC_SCAN, 10240, Time (ms) to perform scanning for limited "discovery" procedure.
=> it seems to be for the above 1 and 2.
13. TGAP_CONN_SCAN_INT, 480, Scan interval used during Link Layer Initiating state, when in connectable mode(n * 0.625ms)
14. TGAP_CONN_SCAN_WIND, 240, Scan window used during Link Layer Initiating state, when in connectable mode(n * 0.625ms)
=> Does this mean that the "in any discovery or connection establishment procedure when user initiated." ?
15. TGAP_CONN_HIGH_SCAN_INT, 4-16384, Scan interval used during Link Layer Initiating state, when i connectable mode, high duty scan cycle scan parameter(n * 0.625ms)
16. TGAP_CONN_HIGH_SCAN_WIND, 4-16384, Scan window used during Link Layer Initiating state, when i connectable mode, high duty scan cycle scan parameter(n * 0.625ms)
=> it seems to be used when high duty cycle scanning and connection initiating by using directed connection establishment procedure. right?
17. TGAP_GEN_DISC_SCAN_INT, 16, 4-16384, Scan interval used during Link Layer Scanning state, when in general discovery procedure
18. TGAP_LIM_DISC_SCAN_INT, 16, 4-16384, Scan interval used during Link Layer Scanning state, when in limited discovery procedure
19. TGAP_GEN_DISC_SCAN_WIND, 16, 4-16384, Scan window used during Link Layer Scanning state, when in general discovery procedure
20. TGAP_LIM_DISC_SCAN_WIND, 16, 4-16384, Scan window used during Link Layer Scanning state, when in limited discovery procedure
=> Is this for "in any "discovery" procedure", not "in any connection establishment procedures"?
21. TGAP_CONN_EST_SCAN_INT, 16, 4-16384, Scan interval used during Link Layer Initiating state, when using connection establishment procedure
22. TGAP_CONN_EST_SCAN_WIND, 16, 4-16384, Scan window used during Link Layer Initiating state, when using connection establishment procedure
=> Is this for "in any connection establishment procedures" or scanning for another devices after connected ?
And should the scanning duration be matched with the scan interval * 3 channels?
if scan interval is 30 ms, 30ms * 3 channels = 90 ms?
Thanks in advance for your answer.
Ji Won