This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC264-indication failure

Hi:

I'm modifying multi-role demo project, and attend to use one characteristic to indicate data change. But it looks like that there are something wrong. I use Packet Sniffer captured the packet:

 my code is as follows:

uint8_t test[] = "12345";
static attHandleValueInd_t ind;
void processSendReq(void)
{
  uint8_t ret;

  ind.pValue = test;
  ind.len = 6;


  //the code don't finish ,and only can communicate with the first device connected.
  ret = simpleProfileIndicate(connHandleMap[0], &ind, selfEntity);
}

bStatus_t simpleProfileIndicate( uint16 connHandle, attHandleValueInd_t *pInd,uint8 taskId )
{
  uint16 value = GATTServApp_ReadCharCfg( connHandle, wechatProfileChar2Config );

  // If indications enabled
  if ( value & GATT_CLIENT_CFG_INDICATE )
  {
  // Set the handle (uses stored relative handle to lookup actual handle)
  pInd->handle = simpleProfileAttrTbl[WECHAT_CHAR2_VAL].handle;

  // Send the Indication
  return GATT_Indication( connHandle, pInd, FALSE, taskId );
}

return bleIncorrectMode;
}

So,  who can tell me where I go wrong?