This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No ring indication cc2564x

Other Parts Discussed in Thread: CC2564

Hello.

I am trying to get the ring indication and in-band ringing on the remote headset. My setup is the following:

1) Jabra Headset

2) CC2564 which is used as a gateway server.

The pair and bond sequence is the following:

1) Pair CC2564 with the headset.

2) Discover an audio port ID.

3) Issue VS_PCM_Codec_Config_Slave_I2S command.

4) Start Audio Gateway Server with HDSET_Open_Audio_Gateway_Server_Port API call.

5) Register SDP record with HDSET_Register_Audio_Gateway_SDP_Record API call.

After this initialization procedure I able to get the events from the headset (button press, gain change, etc) and get the PCM sound from the microphone, also I can play any sound on the headset but only after the headset button was pressed.

When I try to use HDSET_Ring_Indication command nothing happens - the headset doesn't indicate anything.

May be my setup sequence is incorrect? Could someone give me some tips?

Thanks.