Hi All,
I want to work with cc1350(BLE and sub 1-GHz), I looked at the Dual mode example(rfWsnDmConcentrator,rfWsnDmNode), the dual mode example using EasyLink, also the example dos't fit our use case, i have question about using simple_peripheral and sub 1-GHz drive:
1- Can i use the simple_peripheral as it is with RF_driver? simple_peripheral for BLE, the RF_driver will handle the sub 1-GHz.
2- In the simple_peripheral example there is no calling for RF_open(), how it possible?
3- If the simple_peripheral call RF_open() and open client to the RF driver, can i also open another driver to the sub 1-GHz with sub 1-GHz parameters?
4- What is the best way to combine the BLE and sub 1-GHz?