Hi,
Greetings of the day!!
We do have 24-bit DSP Audio Mixer unit.Audio mixer unit that provides HIFI quality intercom between several users., with external BlueTooth connectors. Each user will carry a headset, which can be connected to these connectors. At the same time the user must be able to connect a mobile phone, which they can switch to, if it rings. Or if no audio mixer available, but another similar headset user, they must be able to pair the 2 headsets, and still have each mobile phone connected. In this case one must be HFP agent, and the other must be HFP-AG agent. "
So as per knowledge we just need below functionality
1)Create a feature using the long range BT module with simultaneous SPP(Mobile phone connectivity) and HSP connections.
2)Set up a simultaneous A2DP and SPP connections from smartphones to a BT module(Which need to be select)
One smart phone should establish the A2DP connection for streaming stereo audio to the BT module and in addition to establish an SPP connection for a low bit-rate data transmission to the BT module UART.
3)Our requirements could be with 10-16dBm BT module. This requires class 1 type BT which have maximum gain of 20dBm or 100mW.
4)About 10-16 dbm BT module.. What we require is a range of 300 - 500 meters Line Of Sight between two headsets... We can add a 1-2 dbm antenna. So we can work on power ( dbm ) sensivity, sampling etc. to get the desired range.
I would like to request you to provide me support for suitable BT module with Stack availability for simultaneous connections..
Thanks
Dinesh Katkar