Hello,
There is much information about the low (~1uA) current consumption of CC2540 based devices when performing the Peripheral role, but little said correspondingly for the Central role. On searching the Ti E2E database I did come across a reference to this issue in which the definition POWER_SAVING is made, which presumably forces standby mode. However, I am unsure where exactly this should be defined. I have tried defining it in main() of the SimpleBLEPeripheral project, but to no avail - the current drain between RF bursts is a steady 0.5mA, indicating 'idle' rather than 'standby' mode.
Can anyone please advise?
Best regards,
Caleb.