Hai
i would like to know the following details about TI's cc2540 Ble module.
1. what will be the current consumption when it transmit at maximum power and 10sec of TX interval............?
2. is it possible to get the MAC address of a device when it is connected to cc2540.........?
3. if it is possible to get the MAC can i store the mac in non-volatile memory..............?
4. can i use cc2540 to transmit some sensor data without connect to it like beacon or broad cast...............?
5.if it is possible to broad cast data can i use a second cc2540 to read this data and perform some actions based on this data.............?
6.how many analog and digital i/o pins are there. i found from the datasheet that there are 21 GPIO's........?
thank you