Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640
Hi,
I see at SensorTag and sensortag_cc2650lp_app, there is ccservice.c. Reading the header it say this below. So for CC2640 based end product I need to use ccservice to work with iOS and Android based devices? If I am using project zero as base for product development, I would need to add this as one of the profiles?
"This file contains the proprietary Connection Control Service for use
with the sensor tag application to enable functionality limited by iOS
Core Bluetooth and Android BLE."
- kel