This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640: Code size - code in external storage

Part Number: CC2640


The CC2640 has 128kb internal flash.  I initially assumed that an external flash could be used for additional code space, though I knew it wouldn't run as fast from an external flash.

After digging into the specs, examples, forums ... that doesn't look possible, but I've never heard it directly said.  Could someone confirm that it is NOT possible to use an external flash device to increase one's potential code size appreciably or if it is possible, tell me how to do it?