Other Parts Discussed in Thread: CC2640, CC2650
Hi All,
I made a custom board with cc2640, it can run well in debug mode. In standalone mode, the discovery/paring are hardly, only few times can successfully.
I had checked:
Reset - it is OK, because the led can twinkling every 5 seconds. The resister i tried 4.7k/10k/100k, capacitor is 0.1uF
Power Pad - it has soldered, and connected to ground
I use chip antenna, and balun.
Is the problem impedance matching of antenna?
Thanks for help