Other Parts Discussed in Thread: CC-DEBUGGER, TPS793, CC2511
I am currently a high school student that is taking a year long engineering class. In this class we work on one project all year. Right now we are at a phase where we need to flash a certain hex file onto the cc 2541 using a cc debugger. The only problem is that i can not get the cc-debugger to detect the chip. The cc 2541 chip is on an HM-11 Bluetooth chip and we put the HM-11 on a breakout board. I have read the cc-debugger manuel countless times and i don't know what i am doing wrong. We are using the cc-debugger to power the chip as well. Do i use the simple set up where i just plug in all the pins to the breakout board without using resistors and transistors or do i have to use them ?
Thanks, help is much appreciated