Part Number: CC2640R2F
Hi,
I wanted to ask about the new CC2640R2F.
If I understand correctly by using this chip there is more space for Application code,
due to stack moving from in-system flash to ROM.
1. Can I run old firmware\products which are using stack(2.1.0) on this chip without porting to stack 3.0.0 or is stack 3.0.0 a must for this chip.?
2. Trying to understand how much memory from the comparrison in the datasheet.
Table 3-2. (pg. 5) Typical(1) Flash Memory Available for Customer Applications
http://www.ti.com/lit/ds/symlink/cc2640r2f.pdf
Question:
Are the values mentioned in the table the leftover space for code, after placing the applications mentioned there in the remarks(2,3)?.
Thanks
Regards,
Tamir