Other Parts Discussed in Thread: CC2640
Hi
Just want to know If I missed something.
I changed stack version from [ble_cc26xx_2_01_01_44627] to new [SimpleLink™ CC2640R2 SDK 1.00.00.17.eng]
And at the same time changed chip version to R2 of CC2640
I have followed your guide how to do this and when I got my code running again I see that "just works pairing" doesn't work anymore.
Here are my settings. (same settings in both central and peripheral. Only different is that Central uses GAPBOND_PAIRING_MODE_INITIATE )
// GAP bonding settings.
{
uint32 passkey = 0; // passkey "000000"
uint8 pairMode = GAPBOND_PAIRING_MODE_WAIT_FOR_REQ;
uint8 mitm = FALSE;
uint8 ioCap = GAPBOND_IO_CAP_NO_INPUT_NO_OUTPUT;
uint8 bonding = TRUE;
uint8 autoSyncWhitelist = TRUE;
GAPBondMgr_SetParameter( GAPBOND_DEFAULT_PASSCODE, sizeof ( uint32 ), &passkey );
GAPBondMgr_SetParameter( GAPBOND_PAIRING_MODE, sizeof ( uint8 ), &pairMode );
GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof ( uint8 ), &mitm );
GAPBondMgr_SetParameter( GAPBOND_IO_CAPABILITIES, sizeof ( uint8 ), &ioCap );
GAPBondMgr_SetParameter( GAPBOND_BONDING_ENABLED, sizeof ( uint8 ), &bonding );
GAPBondMgr_SetParameter( GAPBOND_AUTO_SYNC_WL, sizeof ( uint8 ), &autoSyncWhitelist );
}
Tried to attach an air sniffer bot your forum doesn't let me attach an .cfa. How do I attach an air sniffer for you?
I only get pairing failed with unspecified reason.
Have you changed anything in the stack API in the upgrade that I have performed?