Other Parts Discussed in Thread: CC2650
I have added the FCC test into my code, reference to
1) Connect to cc2540.
2) Issue command to
a) turn off advertising
b) enable flag for button to cycle FCC tests
3) Press button to cycle tests.
I hooked up a power meter, and measure power output for each of the test freq, and nothing measured.
Also, testFMode is assumed to be testMode.
It mentioned device sleep. Do I put the device to sleep after issuing command?
For FCC tests, can I have a simple code just for FCC testing. Does it have to be final code as released to customer, or just a test of hardware.