Part Number: LAUNCHXL-CC2650
Tool/software: TI-RTOS
Hello,
I am working on multirole project (Stack : 2.2.1)
I have connected two peripherals to multirole and a mobile phone.
I have observed following issues.
1.) MultiRole Successfully discovers the peripherals. And also successfully gets connected with these devices.
But I have also observed sometimes after the Discovery of peripherals connection to these devices gets terminated immedietly after connecting.
In which case I have to re flash the multi role project.
2.) I am using Android App nRF Connect from Nordic Semiconductors to connect with the multirole.
Discovering of multirole and connection to multirole happens successfully. But there is a frequent disconnection happening.