Part Number: CC2564MODA
Other Parts Discussed in Thread: CC2564, CC2564C, CC2560,
Hi,
In an new projet, i have to make a bluetooth connection with a smartphone.
We need to transfert audio and data.
For audio, we will use A2DP or HFP v1.6. (Unassisted ??)
For data, we want to use SPPLE profile.
Is it possible to use the two profiles at the same time ?
I have found contradictory informations :
In wiki.to :
We support the CC256x device which include the CC2560 and CC2564 and CC2564C. The CC2560 is BT 4.1 without BLE support. The CC2564 is BT 4.1 + BLE (BT 4.2 + BLE for CC2564C), which means it can do both Classic Bluetooth and BLE at the same time. In addition, the CC256x can do ANT+ as well but not at the same time as BLE. Thus our device supports Bluetooth + Bluetooth Low Energy or ANT.
in TI CC2564MODA datasheet:
ANT and the assisted modes (HFP 1.6 and A2DP) are not available when Bluetooth low
energy is enabled.
Thanks.
Olivier.