Part Number: CC2650
Hi,
Last week I asked about getting the UART to BLE bridge example (spp_ble_client and spp_ble_server from the ti-simplelink/ble_examples archive on GitHub) working on a pair of CC2650EM that are included with the SmartRF06 eval kit. Since I wasn't making any progress I went ahead and ordered a couple of CC2650 LaunchPad's, since that is the original target for these examples.
Unfortunately I have the exact same problem on the LaunchPad: The client seems to work fine (can debug, blinks LED's as expected etc), but the server becomes immediately unresponsive on the call to BIOS_start() and ends up in an infinite loop at address 0x1001bbd6, which I understand is the default TI RTOS CPU exception handler.
Some background:
- I am using Code Composer Studio 7.0
- I flashed the "spp_ble_server_cc2650lp_stack" project first, then flashed the "spp_ble_server_cc2650lp_app" project
- The TIRTOS version is 2.20.1.8
If anyone has some things I could try to ge tthis working I'd be very grateful.
Regards,
Jeroen