This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540: cc2540 as 1-wire slave

Part Number: CC2540

I am trying make the cc2540 act as a 1-wire slave device. I can send a presence signal on reset, get a ROM read, but have trouble writing back the ROM information.

I have setup interrupts to HIGH-LOW edge trigger. When I get the edge, I want to hold it low, to send a zero bit.

Problem, is in 6us, the master releases the data line, which is too fast, as I send low to the line, but it takes 12us till it goes low.

Is it possible to do 1-wire communications on cc2540?