Part Number: CC2560
Hello,
I am developing a product based on your HFP Demo.
There is no problem in SCO connection with android phones.
But I am failing in SCO connection with iPhones.
The iOS is 9.3.5.
When I issue ManageAudio 1,0 on prompt,
I got the message like the below:
manageaudio 1 0
HFRE_Setup_Audio_Connection: Function Successful.
HFRE16>
HFRE Audio Connection Indication, SCO/eSCO handle: 0xf000 HFP ID: 0x0001, Status: 0x0001.
I2S configuration start f = 8000
Setup CVSD with Audio for ACL handle 0x0
ServerPortIndex : 1.
IsConnected : TRUE.
IsCallWaiting : FALSE.
IsCallOnHold : FALSE.
IsInActiveCall : FALSE.
IsInActiveSCO : TRUE.
IsInActiveAudio : TRUE.
I have posted a question related to this last year.
But it disappeared from this forum.
Could you have any solution or suggestion I can try?
Thank you.