Part Number: CC2564
Other Parts Discussed in Thread: TM4C123GH6PZ, CC256XM4BTBLESW
Tool/software: Code Composer Studio
Gentlemen,
IDE is CCSv7 in Windows. Hardware is TM4C123GH6PZ connected to a PAN1326B (CC2564B) on a custom board.
I'm trying to implement the Bluetopia (CC256XM4BTBLESW) into our existing firmware, to add, initially, BT classic SPP communication. Our existing firmware uses TivaWare, and NOT TI-RTOS.
Given the specific board, the fact that there is already a whole firmware working "for the rest of the product", and that I do not own a TM4C129X evaluation kit just to see Bluetopia running on the example's environment, I'm having a hard time to achieve my goal. The WIKI example is way specific for the example to run, but it mentions nothing regarding porting the stack into one's existing project.
Is it possible for the TI fellows here to provide some guidance for such mission? Some questions:
- Given that I get the paths sorted out on my project configuration, which headers exactly do I need to include?
- Because I'm noOS, it appears that I need to create my own functions for some basic tasks: ready system elapsed milliseconds (no problem) - and also for other things that I would not expect, such as to initialize a memory section with a certain value. Is that really the case?
Any further literature or real-life examples for this implementation will be much appreciated!
Regards
Bruno