This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650STK: Getting RSSI value and converting it to dbm

Part Number: CC2650STK
Other Parts Discussed in Thread: CC2650

I am currently doing a project on using the cc2650 sensortag to do a simple proximity for tracking children up to 10m on a nexus 7 android sdk 21 system. 

I wish to test out some research paper formula however it requires the RSSI reading to be converted to dbm value. 

Is there anyway to do it ? i am not allowed to do any modification to the sensortag code, it currently using the default sensortag project in the BLE stack (2 - 2- 1).

I been using readRemoteRSSI on the android side to get the RSSI value.

Or is there any other way beside this method that i can achieve this, any help would be greatly appreciated.