This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: In CCS7 I can't deselect the options when importing CCS example projects

Tool/software: Code Composer Studio

I have Code Composer Studio  Version: 7.0.0.00043

Have installed SimpleLink CC2640R2 SDK Version 1.00.00.22

When trying to import any of the projects from "C:\ti\simplelink_cc2640r2_sdk_1_00_00_22\examples\rtos\CC2640R2_LAUNCHXL\blestack" the options "Automatically ..." and "Copy projects into workspace" gets  greyed out with the "Copy project into workspace" is selected
it is now not possible to deselect the option.
Why?  I dont want the project copied into my workspace.

BR
Örjan Christensson