Part Number: CC2650STK
Other Parts Discussed in Thread: CC2640, , CC2650
Dear TI Community,
We are developing a Firmware for a customer board which with a CC2640. We ported the CC2650STK SensorTag firmware on this board but now we could observe a strange issue:
The firmware is running on the customers board; as a central device we use the SmartRF06 with CC2650EM. In btool we set the following Connection Parameters:
Connection Interval: 1600 (2000 ms)
Slave Latency: 4
Supervision Timeout: 3200 (32 000 ms)
When connecting to the customer’s board we get a supervision timeout after 32 seconds. Even though we measured a connection event every 2 seconds.
The same firmware running on the CC2650 SensorTag gets no Supervision Timeout and the connection stays stable all the time.
Could anyone explain this?
Unfortunately we don’t have a USB dongle, so we cannot use TI’s Packet sniffer.
Thanks
Steffen