Part Number: CC2640
I have a SimpleLink Academy ProjectZero modified to access external flash for data storage purposes.
It has been working fine but I have now noticed this issue. The second time I try to open the OAD_target, the function returns 0 and I am unable to figure out why.
My program is big enough that I have to disable all logging and can't even set it up for ROV anymore. I have been building with optimization OFF so that breakpoints work better. So, with a breakpoint after the following code I can see that did2 was never set to 1.
By setting breakpoints, I have been able to determine that the second time OADTarget_Open was called, the ExtFlash_readInfo() routine did not provide the correct 'devicesize,manfD,devID' that it did the first it was called in pFlashInfo.
Why would this happen?
Thanks,
Dale
uint8_t did1 = 0;
if (OADTarget_open()) {
did1=1;
}
OADTarget_close();
uint8_t did2 = 0;
if (OADTarget_open()) {
did2=1;
}
OADTarget_close();