Part Number: EZ430-RF2500
Tool/software: Code Composer Studio
Hi,
I'm using a PAN1323 Blutooth-Module, which is based on CC256x-Controller, to setup a HFP-Bluetooth-connection.
Therefor I'm using the HFPDemo-project and want to configure the sound-data to be transfered via I2S-interface and the control command via HCI.
As I already know, I'have to use the CC256x_VS_HCI_Commands, espacially HCI_VS_Write_CODEC_Config_Enhanced (0xFD07) to configure the interface, but I'm not clear how and where this command has to be included.
What would help me best, would be a sample, that shows a I2S-Interface used at a Bluetooth-connection.
With best regards