This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640: OAD Image reject

Part Number: CC2640


Hi,

I am doing on-chip OAD on cc2640. I made Image A and it is working fine with other project Image B. I need Image B for default simpleBLEPeripheral project. I made all the changes given in CC2640 OAD Developer Guide in SimpleBLEPeripheral project. But when i trying to download it using BLE Device Monitor App. it showing OAD IMAGE Rejected.

09:32:50.476 > OAD started
09:32:50.491 > WriteRsp[FFC1]: st=0 n=0
09:32:50.500 > Notif.[FFC1]: st=0 n=8 00 00 80 16 41 41 41 41
09:32:50.500 > OAD image rejected

  • Hello,

    I've asked our OAD expert to look into this. In the meantime, I suggest using the debugger to identify the reason this is being sent in your application.

    Best wishes
  • Aditya,

    You mention using another project Image B, which project are you referring too?

    The simple_peripheral project already has a IMG_B configuration to use with all all changes mentioned in the guide done already; can you verify if this works?

    Regards,
    Rebel