This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: CC2650

Part Number: CC2650

Hi All!

I am just have the following questions:

  1. BLE and ZigBee Stacks are concurrently working? Or one single at time?
  2. If the stacks have to be switched.
    1. What is the transition time?
    2. Is there a time limit to stay on the current stack?
    3. Does your implementation automatically switch the stacks? OR Does the application have to do it?
    4. Are the stacks capable to share information between each other?
    5. Do the stacks can be switched back and forth any time? OR Once the stack was switched it cannot be switched anymore?