Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2650, SYSBIOS
Tool/software: TI-RTOS
Hi
We are getting short of RAM in our SW.
Our setup:
- CC2640R2F
- Stack in ROM.
- BIOS in FLASH
- Currently Application and Stack in 2 binaries (Stack not yet in library - but does this really help us save RAM?)
Can you confirm this assumption from us? "From the 20K chip RAM, the BLE Stack and ROM uses 3936 bytes (-D ICALL_RAM0_START=0x200040a0)"
Is there anything we can do about this value?
If this is fixed we have appr 16 KB RAM left for our "application".
Here is a part of our MAP-file pointing out the RAM-consumption for our application (we have hidden our object's names - and those are of course our responsibility), and we wonder if there is anything that one can see that one can optimize? We feel that from the 16 KB RAM left (see the ICALL_RAM0_START above) the TI code (stack, bios, gap/gatt) we are really left with small fractions.
Things that we wonder about are e.g.:
app_ble_prm3: appr 3 KB
devinfoservice: 500 bytes (is this mandantory according to BT spec?)
icall: 280 bytes
peripheral: 800 bytes (source taken from the example code, needed for GAP, but we have not made any attempt to modify it - maybe we can optimize this?)
RFCC26XX_singleMode: 550 bytes
We have an idle task stack size of 512 bytes, but we believe that this can be cut in half? When we run our code it looks like a high-water mark on this stack usage is appr 170 bytes. Maybe we don't need the idel task at all?
We have also have noticed that If pairing should work we need to allocate at least 2800 bytes to heap (HEAPMGR_SIZE=2800)
Questions (again);
? 1 ? Is it true that we have appr 16 KB for the Application (after the ROM stack has taken its share)? Can we do anything to increase this figure?
? 2 ? The 5 sw objects lifted out from the MAP above, does it seem plausible regarding the RAM consumption? Can we do anything to decrease those figures?
? 3 ? Do we really need the idle task? If so, we think we can at least strip away 256 bytes from its stack.
? 4 ? Is the HEAP size of 2800 reasonable? We need pairing to work.
the MAP file...
*******************************************************************************
*** MODULE SUMMARY
***
Module ro code ro data rw data
------ ------- ------- -------
C:\Data\GIT\MowerBLE\SW\Bluetooth\Peripheral\App\Config\configPkg\package\cfg: [1]
app_ble_prm3.orm3 1 100 1 416 3 158
----------------------------------------------------------
Total: 1 100 1 416 3 158
C:\Data\GIT\MowerBLE\SW\Bluetooth\Peripheral\App\HVHMIBoard\Obj: [2]
XXXXXXXXXXXXXX0.o 148 56
XXXXXXXXXXXXXX1.o 2 496 360 677
XXXXXXXXXXXXXX2.o 592 96 4
XXXXXXXXXXXXXX3.o 1 844 591 964
XXXXXXXXXXXXXX4.o 388 92
XXXXXXXXXXXXXX5.o 136 12
ECCROMCC26XX.o 1 184 5
XXXXXXXXXXXXX10.o 2 500 716 29
XXXXXXXXXXXXX11.o 872 108 24
XXXXXXXXXXXXX12.o 80 4
XXXXXXXXXXXXX13.o 6 720 32 1 181
XXXXXXXXXXXXX14.o 328 28 264
XXXXXXXXXXXXX15.o 240 288
XXXXXXXXXXXXX17.o 1 310 272 420
XXXXXXXXXXXXX18.o 136 664
XXXXXXXXXXXXX19.o 388 51 248
XXXXXXXXXXXXX20.o 376 281
XXXXXXXXXXXXX21.o 156 8
TRNGCC26XX.o 352 1
XXXXXXXXXXXXX22.o 184 16
XXXXXXXXXXXXX23.o 1 888 28 656
Watchdog.o 44 4
ble_user_config.o 34 226 16
board.o 64 129
ccfg_appBLE.o 88
devinfoservice.o 404 232 494
gatt_uuid.o 8
gattservapp_util.o 788
icall.o 3 484 30 280
icall_api_lite.o 88 8
icall_cc2650.o 316 2 5
icall_user_config.o 94 16
main.o 76 7 16
peripheral.o 4 312 20 801
XXXXXXXXXXXXX25.o 224 1 113
----------------------------------------------------------
Total: 36 552 3 513 8 776
C:\Data\GIT\MowerBLE\SW\Bluetooth\simplelink_SDK\source\ti\blestack\rom\ble_rom_releases\cc26xx_r2\Final_Release: [3]
----------------------------------------------------------
Total:
command line: [4]
----------------------------------------------------------
Total:
boot.arm3: [5]
boot.orm3 22
cmain.orm3 26
cstartup_M.orm3 22
iar_xdc_init.orm3 32
----------------------------------------------------------
Total: 102
dl7M_tln.a: [6]
abort.o 6
div.o 14
low_level_init.o 4
rand.o 55 140
snprintf.o 68
sprintf.o 52
srand.o 32
strrchr.o 24
vsnprint.o 60
xprintffull_nomb.o 3 538
xsnprout.o 26
xsprout.o 10
xtls.o 2
----------------------------------------------------------
Total: 3 836 55 140
dpl_cc26x0r2.arm3: [7]
HwiP_tirtos.orm3 8
PowerCC26XX_tirtos.orm3 220
----------------------------------------------------------
Total: 228
driverlib.lib: [8]
adi.o 48
chipinfo.o 54
cpu.o 24
driverlib_release.o 1
interrupt.o 48 200
ioc.o 104
osc.o 252 20
rfc.o 162
setup.o 292
sys_ctrl.o 676 8
uart.o 152
----------------------------------------------------------
Total: 1 812 229
drivers_cc26x0r2.arm3: [9]
CryptoCC26XX.orm3 1 086 29
List.orm3 60
PowerCC26XX.orm3 1 928 107 272
PowerCC26XX_calibrateRCOSC.orm3 1 184
----------------------------------------------------------
Total: 4 258 107 301
m7M_tl.a: [10]
DblAdd.o 212
DblCmpGe.o 46
DblCmpLe.o 46
DblDiv.o 598
DblMul.o 418
DblSub.o 384
DblToI32.o 88
I32ToDbl.o 48
xdnorm.o 68
xdscale.o 268
----------------------------------------------------------
Total: 2 176
rf_singleMode_cc26x0r2.arm3: [11]
RFCC26XX_singleMode.orm3 4 264 551
----------------------------------------------------------
Total: 4 264 551
rt7M_tl.a: [12]
ABImemclr.o 6
ABImemclr4.o 6
ABImemcpy_unaligned.o 118
ABImemset.o 102
ABImemset48.o 50
I64DivMod.o 238
I64DivZer.o 2
data_init.o 40
lz77_init_single.o 120
memchr.o 88
strchr.o 22
strcmp_unaligned.o 66
strcpy_unaligned.o 68
strlen.o 54
zero_init3.o 64
----------------------------------------------------------
Total: 1 044
shb_l.a: [13]
exit.o 20
----------------------------------------------------------
Total: 20
sysbios.arm3: [14]
BIOS.o 6 640
m3_Hwi_asm_iar.obj 268
m3_Hwi_asm_switch_iar.obj 104
m3_TaskSupport_asm_iar.obj 108
----------------------------------------------------------
Total: 7 120
Gaps 9 8 1
Linker created 16 40 1 024
--------------------------------------------------------------
Grand Total: 62 537 5 139 14 180