This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Starterware/CC2564C: Source code for Bluetopia Platform Manager Linux add-on running either with Sitara starterware or Linux

Part Number: CC2564C
Other Parts Discussed in Thread: CC2564

Tool/software: Starterware

I am on a tight schedule and need to demonstrate our new MCU based on BBGW reference design, interacting with multiple peripherals including talking to an iPhone using BLE 4.2 using the CC2564C asap.

Would it at all be possible to get access to the source/drivers used for TI-BT-STACK-LINUX-ADDON so that I can customize it for our baremetal environment? If so can I expedite this via our TI account manager?

Any suggestions on the fastest approach to get this up and running?

PS: Long term we will be using the Bluetopia PM Linux add-on in a custom Linux environment.

  • Hi James,

    James Pereira said:

    Would it at all be possible to get access to the source/drivers used for TI-BT-STACK-LINUX-ADDON so that I can customize it for our baremetal environment? If so can I expedite this via our TI account manager?

    The source code of the TI dual-mode Bluetooth Stack is not generally provided and because of the porting required for baremetal environment, I would not recommend going this route since you mentioned you are under tight timeline. 

    James Pereira said:

    Any suggestions on the fastest approach to get this up and running?

    Yes, using Linux (ti processor SDK for Linux or the Debian distribution that comes with BBGW) are your fastest option to get it up and running.

    James Pereira said:

    PS: Long term we will be using the Bluetopia PM Linux add-on in a custom Linux environment.

    Is there a reason why you cannot use Linux right now?

    Best regards,

    Vihang