Hi,
I am using the Simpleble central project on the eval board.I use an android app as the advertiser and once conenction is established, I observe the EMPTY_PDU packets on the sniffer.
My observvation is that these packets are at a constant interval of 100ms from the Master (Eval board) but only 200us from the Android app.
Which parameter should I change to bring down the 100ms interval to say 1ms? Also, would it imrpove my connectivity performance. I understand that power consumption would increase,
-Sayu